Hi,
I would like to ask you how to use the LP5018.
(question 1)
Is it okay to understand that the current can be adjusted for each of the 18 LEDs?
Is current adjustment a method of changing the current value itself? Or is it a method of changing with PWM?
(Question 2)
Is the maximum LED current determined by RIREF and applies to all LEDs?
(Question 3)
Up to 18 LEDs can be connected. And I want to light 3 or 6 at the same time. Is that possible use?
(Question 4)
How many LEDs can be turned on at the same time?
(Question 5)
When turning off only a specific LED, should the brightness register of the corresponding LED be set to 0?
Best regards,