This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS791: Find TI's solution

Part Number: TPS791

Please check whether TPS719 is the best solution for MM3816A18, MM3816A25, M3816A33, since the dropout voltage is slightly different.

Does TI has other p2p solutions?

 

P/N

Core function: Iout

Vout(V)

PKG

Dropout V (mV)

Max Vin (V)

Noise (uVrms)

Features

MM3816A18RRE(R59-AX90)   1PCS/PCBA

200mA

1.8

PLP-4C

350

6.5

60~90

enable, discharge

MM3816A25RRE(R59-AX97) 3PCS/PCBA

200mA

2.5

PLP-4C

280

6.5

60~90

enable, discharge

MM3816A33RRE(R59-AY06) 8PCS/PCBA

200mA

3.3

PLP-4C

210

6.5

60~90

enable, discharge

TI's product

 

 

 

TPS719 (P2P=N)

200mA

1.8/2.6/3.3

WSON 6

230

6.5

84

enable, discharge