This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM27761: lm27761 Load issue

Part Number: LM27761

Dear TI,

I am using LM27761 to supply negative 5V sensor. I have this issue that without the load I can see -4.86V at Vout but when I power up with the sensor negative pin attached to Vout then I started to see around 0.3V only but when I removed the sensor and placed back again then the voltage come back to -4.86V.

Sensor current is only 30mA and is required that it is always attached to Vout. May I know what is the reason for this load issue? I followed the same component values as indicated in the datasheet.

Thank you for your help.

Regards,

Leo