This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61200: Design Advice

Part Number: TPS61200

Hi,

I was trying to test the TPS61200 so I designed and assembled the circuit shown below: Vout=5.5 V. However, I am not getting any output (no voltage) under no load or load conditions. Also, the circuit consumes a lot of current even when no load is connected: e.g. Vin=5V, Iin=46 mA. Do you have any comments on my design or most likely was an assembly issue? Any advice for troubleshooting this will be greatly appreciated.

Note: I added a LPF at the input but I don't think this will be an issue.