Dear support team!
I would like to implement a Soft-Start with the LM46001. Normally it is recommended to use an external capacitor to set the soft-start time.
An internal current source will load this external capacitor until a voltage of 1V is reached. In our application we need a startup time of ~45ms.
Therefore a 100nF capacitor is needed.
Is there the possibility to reach this 45ms soft-start time with a lower value capacitor (e.g.: with a parallel resistor)?
Then we can use a C0G/NP0 ceramic-capacitor with lower tolerances.
Kind regards,
Markus