Hi,
when over(out of range) temperature and recover temperature detected Bq27510-g3 Gpout pin not toggle.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
when over(out of range) temperature and recover temperature detected Bq27510-g3 Gpout pin not toggle.
Hello Ankit,
Make sure you have configured the gauge correctly for this operation. You can reference this post for more information: e2e.ti.com/.../923676
the GPOUT pin as a lot of functionality and has to have multiple registers configured to get the desired operation.
Can you send the .gg file and log of your tests?
Sincerely,
Wyatt Keller
Hello Ankit,
In the post I linked above it discusses how to setup the op config register for the same application (charge control based on temperature). I checked the .gg file posted here and it looks like the op config is still the default values, you will need to configure them like mentioned in the other post.
GPOUT_INT = 0
BAT_FN = 1
PFC_CFG[1:0] = 01
Also select GPOUT_POL as desired.
Sincerely,
Wyatt Keller