Other Parts Discussed in Thread: LM25141
Hi Support team
Based on my applications (Vin_typ=24V, Vo=13.5, Io=10A, fs=440kHz), a 4.7uH inductor is selected to meet about 30% ripple current.
However, according to Equation 13, the inductance should be greater than10uH.
The inductor ripple current will be only 13% if a 10uH inductor is used. And this is conflict with the assumption of 30% ripple current.
Could LM25141-Q1 work well with a 4.7uH inductor in my application? Thank you.