Dear TI Team
The LP5024 data sheet introduces a form in which a voltage is applied to each OUT terminal from a single Vled.
However, customers are considering a method of driving one LP5024 by changing the number of LEDs to be connected for each out terminal.
For example, is it possible to apply different values of power supply voltage (Vled) for LED lighting to each OUT terminal as shown below?
(Turn on multiple voltage LED drive power to one LED driver)
Example
OUT1: One LED alone ← 5V input (Vled)
OUT2: 2 LEDs in series ← 7.5V input (Vled)
OUT3: 3 LEDs in series ← 12V input (Vled)
Best Regards,
Y.Ottey