This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5163-Q1: quiescent current

Part Number: LM5163-Q1
Other Parts Discussed in Thread: LM5163

Hi Team,

I received the following request, could you assist?

####################################################

 

We use LM5163-Q1 to convert the battery 24V into regulated 5V.

The datasheet indicates the following consumption in "low power":

–10.5-μA no-load input quiescent current

–3-μA shutdown quiescent current

Could you confirm that with the “10.5-μA no-load input quiescent current” the converter (powered by 24V battery) is able to keep the regulated voltage of 5V active?

In fact, we need to keep the microcontroller powered in sleep to be sensitive to some wake-up pulses.

 ########################################################################################

Regards,

Fabio