Hello,
My customer is using TPS62802 and have a question for R_VSEL resistance value.
They need to configure Vout=3.3V.
Table 1. on the datasheet (SLVSDD1E) says “249.0 or larger” for VSEL=16(3.3V).
On the other hand, R_VSEL is defined as MIN(10KOhm)/MAX(249KOhm) in Recommended Operating Conditions.
Is there any problem to use over 249Kohm for VSEL?
Actually the customer is using 270K ohm now. Is it any problem?
Regards,
Oba