This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM4050-N-Q1: Reg: Need to know the LM4050AE-2.5 SPICE model is designed to verify the Reverse Breakdown Voltage Tolerance

Part Number: LM4050-N-Q1

Hi,

I am using LM2050AEM3-2.5 for my application, Hence I want to simulate the behavior of Reverse Breakdown Voltage(±15mV) Tolerance for an Extended temperature range with the test circuit mentioned for Startup Characteristics in Simetrix Environment. But the results -40mV @ 40deg & +51mV @ 105deg which are outside the limits specified in the Datasheet. Check below simulated waveforms for your reference. Also need to to know whether the spice model is designed to simulate the temperature variations or not?. If you not please provide me the specified spice model for Temperature change.

Thanks & Regards

Athieshkumar T