Other Parts Discussed in Thread: LM25141, LM5141,
Hello.
I am having problems with the PSPICE for TI model of the LM25141 which model is LM5141 and I get from www.ti.com/.../snvmau4
I tried with the example “Reference design-->LM5141-Q1RGE_TRANS” and I modified the FB pin by using a voltage divider with 100k to Vout and 11k to gnd, so I expect to see 12Vdc in the output (and 1.2V in FB pin). In the example I also remove the input filter and put an independent voltage source of 30Vdc and finally I put OSC pin to gnd to have 440kHz of SW frequency. (quite similar to the "Reference design-->LM5141-Q1RGE_TRANS")
Voltage in FB pin only reach 0.315V instead of 1.2V that the datashhet of LM25141 as regulation threshold indicates.
In addition in other simulation I connect OSC to the Vdda expecting a SW frequecy of 2.2MHz but I can not see that effect.
Is there any problem with PSPICE for TI or with the model, or I missing something?
I have a problem in a PCB with a buck based on the LM25141 (the duty is no stable) and I think that the simulation should help but now it does not.
Thank you very much.
Carlos.