This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS40200-HT: TPS40200HT component suggestion

Part Number: TPS40200-HT

Hi team,

Good day. Our customer is using TPS40200HT  to achieve three power supplies with an output of 3.3V 5v and 8.25V. They are looking for a  FET and diode that is compatible with their design and would work above 175C. Do you have any parts suggestions? Thank you.


Regards,
Carlo

  • Hi,

    The parts also depend on the load and input voltage, if customer care about 175 TJ they can just choose AEC-Q101 qualified and in manufacture website filter choose 175C for MOSFET (e.g. SQ1431EH, -30V, -3A) and Diode (VS-6TQ035S-M3, 35V, 6A). Normally we don't recommend other manufacture's products for customers which are highly depends on they application. They can choose one and we can help review, thanks.