Hi,
1) I would like to ask that what is the purpose of R58 (1k) and R59(1k) on BQ76940EVM.
I'm asking because, I have seen abnormal current on this line (Example: C10 to VC10X). Therefore, I see changes in cell voltages(Voltage unstability on C10, C11 C12 C13 C14 C15). The problem goes away when I change the resistor(Example R58) with 0 ohm resistor . So I want to know that how important is this resistance?
2) What are the potential negative effects of using 0ohm resistor instead of 1k resistor(R58) on my design?
3) Do you have any idea for voltage unstability? For more details(parts of schematic, etc.) we can use private messages on e2e forum.
Thanks a lot.