Other Parts Discussed in Thread: TPS61089
Hey Team,
I landed on the LMR62014 for my customer's application because it is one of the cheapest boost converters that supports the specs
- Vin = 6.4V-9.4V
- Vo = 12V @ 50mA
Do we have any boost converters that may be better for this applications?
We care mostly about cost and efficiency as to not drain out battery life. It looks like the LMR62014 can only achieve ~85% efficiency at the load specified above. Is there something that can achieve >90%?
Best,
Dajon McGill