Now there is one issue in the field that our BBU cannot charge to 100% RSOC from the log. May I know the reason?
Below is log from the field, the full charge capacity is 12.15Whr, remaining capacity is 10.68Whr. however, from the cell voltage, we can consider it should be reach 100% RSOC from my experience. and our design capacity is 10.56Whr.
Voltage: 10718 Batt pin: 10797 Power cW: 0 ACP mV: 12528
Cell1 mV: 3537 Cell1 mA: 0 Cell1 qmax: 1140 Cell1 bal time: 0
Cell2 mV: 3568 Cell2 mA: 0 Cell2 qmax: 1140 Cell2 bal time: 0
Cell3 mV: 3614 Cell3 mA: 0 Cell3 qmax: 1142 Cell3 bal time: 0
Full Cap cWh: 1215 RSOC: 088 Ave time full: 4800
Remain Cap cWh: 1068 ASOC: 103 Ave time empty: 65535
Gauging Status: 0x00191850 Operation Status: 0x00000197 Battery status: 0x00c7
Charging Status: 0x00010008
One background is that we cannot update Qmax in the field because of the temp limit and 37% delta energy limit. And we will discharge 25% energy and then charge to full every 10 days. I can share you our .gg file by email if you need.