Hello, I have use LM5160-Q1 to make an isolated flybuck converter. The circuit is shown below.
The simulation result looks good. It can control the output voltage to its target value and the process looks nice.
As you can see, V(OUT1) is 8VDC, V(OUT2) is 8VDC and V(OUT3) is 16VDC. The current in the transformer is far beyond 2A.
When I measure the related waveforms on the pcb, although the output voltage gets its target value, they look quit different.
Here is the zoomed simulation waveform when the circuit starts.
The duty of the pulse at SW node is small. And here is the measured waveform.
The yellow waveform is V(SW) and the blue waveform is V(OUT1). The duty of V(SW) is quite large, and it seems to keep such a large duty till the output voltage reaches its target value. Please see the figure below.
I have no idea how to explain this phenomenon. Does the circuit operate normally? I don't think so. What's wrong with it?