Part Number: FUSION_DIGITAL_POWER_DESIGNER
I have a Xilinx AC701 board. I am trying to set GPIO 16 and 17 to '1' via the gui. This should change VCCO_VADJ to 3.3V. I power up the board, bring up Digital Fusion, and then click on configure, and change the settings. I write to hardware and then write to NVRAM. When I cycle power, the board will not come back up. I then have to go back and restore the configuration via provided XML files to restore the board, and bring it back to life.
I am also having issues monitoring the voltages and have played with the SSA settings per other support cases, as well and toggle the control lines via the gui, with inconsistent results!