Hi team,
Can you have a look into the following customer question about PWRON timing?
The TPS65910 is the main PMIC on a single board computer that we use in our system.
I was looking into the timing of the NRESPWRON output. We are characterizing the functional performance of our system and what we’re seeing from the board doesn’t match what I see in the TPS65910 datasheet and app notes, if I’m interpreting the timing correctly. It looks to me like the time from 5V power applied to the PWRON signal should be about 15ms, and we’re seeing closer to 30ms. The single board computer has the chip configured for boot mode of ‘10’.
If you could provide any insight into the timing of that signal, it would be appreciated.
Thank you,
Franz