Hi colleagues,
The PMIC which our customer is currently using for all i.MX53 boards (Dialog DA9053) is facing EOL.
They saw that there are 2+ NXP alternatives but it seems no one can support conversion starting from 5V.
So NXP PMIC need a pre-regulator, at about 3.8V.
It is quiet annoying to the customer to use 2 components instead of one.
They had a quick look into the components and would like to ask a few things:
- TPS659106 is pre-programmed for i.MX53 but needs an external dc-dc converter for DDR3L memories and CPU, is that correct?
For this product they use either WEC7 or Yocto Linux.
- Does this PMICs have both OS drivers?
Best regards,
Candas