This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV62084: Common Power Good signal when using 5 distinct TLV62084A parts to drive power rails into an SoC

Part Number: TLV62084

Hi -

Our board design has 5 distinct voltage rails feeding our SoC:

  • 3.3V
  • 1.8V
  • 1.8V Always ON
  • 0.8V
  • 0.65V

The 1.8V_AlwaysON TLV62084A PG signal feeds the EN pin of the 3.3V TLV62084A and this 3.3V supply feeds the rest if the EN pins (1.8V, 0.8V, and 0.65V) in order to set the power-on sequence.

Our SoC has a 1.8V-level "Power Good" input.

Is it acceptable to connect all of the PG signals from the 3.3V, 1.8V, 0.8V, and 0.65V together with a common pull-up resistor to 1.8V AON?

The intent is that any one of these 4 supplies could pull Power Good low if its voltage fell below the regulation limits. 

Since theTLV62084A PG signal can sink 1 mA, are there any particular pointers as to the value of the common pull-up resistor?

Are there any particular concerns about filtering given that 4 different supplies have the PG signal tied to one node?

Thanks very much,

Tom