Hi,
I want to follow up on another thread:
In the thread, it mentioned to size the diode to 1/2CV^2. I agree that this will be the power dissipated in the diode. My question is that the diode suggested has a forward voltage drop much larger than 0.3V (which is absolute max voltage difference between VIN and OUT (see below)). Wouldn't the IC be damaged? Shouldn't the diode be less than 0.3V? Thoughts?