We are setting EN1 and EN2 high on the BQ51003 to send an EPT packet to the transmitter when our battery charge is complete. However, when we set EN1 and EN2 low again, without removing the device from the transmitter, power transfer will not reinitialize. We have to remove the device from the transmitter and place it back on again to reinitialize power transfer. Is there a message we need to send to the transmitter to reinitialize power transfer if the device never leaves the transmitter? We would like the device to remain topped off if left on the transmitter for extended periods of time.