Other Parts Discussed in Thread: BQSTUDIO, BQ25618
1.Hi team,
am currently working on bq25619 battery,i have a small query regarding charging the internal battery through bat pins
1.What is the voltage i need to get at BAT pins,as my input supply voltage VBUS is 5v
2.Am able to charge the battery upto 3v,later the battery is not getting charged as default setting
in Battery Voltage Limit Register (Address = 04h) is 4.2v as per datasheet mentioned,so my battery has to charge till 4.2v,
but which is not happening
3.what are the registers need to be configured or boost settings need to be done to enable battery charged till 4.2v
4.what are the use of min system voltage in Charger Control 0 Register,is there any co-relation with VBAT Registers