On the LM63610DQPWPRQ1 is spread spectrum enabled? The data sheet seems indicate an option/enable but there is only one part number in the current data sheet.
Related to that..my real question is about subharmonics.
I have a bit more complicated application where I have to do some additional stability compensation.
I am seeing some oscillation/periodic noise in the range 5-20 Khz and I am starting to wonder if it is possible to see the sideband of the frequency modulation of the spread spectrum.
I am using the part at 250Khz, so at 3.5%, that is 7.5Khz.
Bottom line is, can I expect that there would be some noise that is a beat down from the modulation? Or has this been handled somehow?
Thanks
Glen