Hi ,
According to the following schematic diagram parameters R1523 is 30K, R1522 is 7.5K, VBUS=5V, then the Regn also has 5V, and VSYS outputs 1.5V-2.9V oscillation waveform.It can work normally when R1522 is changed to 10K. Could you please help to analyze it?