I’m trying to come up with a metric on how much current will be consumed by the LMG1210 during operation so that I can size my power supplies appropriately. The device has a max sink current of 3A (under the condition of 5V at the gate pin, which does not make sense to me; I would think that it is sourcing current then?) and a max source current of 1.5A. My switch has an internal gate resistance of just 0.6 Ohms, equating to 8A at a 5V gate bias. The app notes do not include any gate resistors, nor does the EVB. Would you recommend gate resistors to limit the current to 1.5/3A, or can I connect it directly to the switch?