Hi Team,
my customer has question about TPS2553 OTP. they measured the Tc and calculate the Tj that is high than 135 degree. But it did not trigger OTP. Please help to explain it.
Below is the info for the testing.
OCP protection parameters
Vin= 3.3V
Vout= 0.05V
Iout= 0.4A
Efuse = (3.3-0.05)*0.4=1.3W
measured Tc= 60ºC
calculated TJ= 60+ 122.2*1.3= 218ºC
After testing, OCP tried to trigger OTP but it failed as below:
Please kindly advise, thanks!
Patty