Part Number: BQ40Z50-R3-DEVICE-FW
Hi,
We are using the bq40z50-R3 in a large format, 4S LiFePO4 pack and are trying to work out why PF faults are being triggered on some packs during charging.
These faults are logged in the Black Box Recorder as;
HWDF in Safety Status/3rd Safety Status C.
CFETF in PF Status/1st PF Status C.
If these faults are related, it may suggest that the charger continues delivering current even after SMBus traffic ceases. This is unexpected, as the CHGFET should prevent this from happening. I have done some testing with bqstudio and an attached regulated power supply (connected as a charger) and confirmed that once SMBus traffic ceases and the 5 second HWD Delay timer subsequently expires, the CHGFET opens and interrupts the charge current, as expected.
I have also tried disabling the CHGFET with bqstudio and measuring leakage current (when the attached regulated power supply was set to the highest recommended voltage for the bq40z50 (26V)), but the FET prevented current flow, as expected.
I have read about similar issues elsewhere in this forum (some apparently still unresolved) and wondered if anyone has any advice or suggestions for troubleshooting this?
How does the gauge detect FET failure?
What does the 'F' in HWDF stand for?
In our application, the host reads Charging Voltage and Charging Current values from the pack and writes them to the Smart Charger once per second.
We have set the HWDF bit in Enabled Protections C to prevent dumb chargers from charging our pack.
Thank you,
Jeremy.