Hi Experts,
I would like to get a load transient response as a following conditions. I tried to simulate it by Webench but Webench does not correspond a simulation for this device. Would you please provide a load transient response by a following conditions?
[conditions]
Vin: 4.1V~6.0V, rated voltage is above 16V.
Vout: 5.1V
Load condition: dozens of mA to 500mA and 500mA to 1.5A
Also I input above condition (Iout max=3.5A) to Webench but it get a following error message. Is this condition unstable?
Best Regards,
Fujiwara