Other Parts Discussed in Thread: TPS552882
Hi Team,
My customer is surveying our buck-boost solution now,
They need:
- Input voltage : 1 cell battery (3V~4.4V)
- Output voltage : fixed 3.3V
- Output current : Imax = 3A
After I search on TI.com, I think the TPS63806 may be the right solution, but the Iout max is 2.5A,
If I want to find a larger solution, our product map will jump to a 16A solution TPS552882, that will be a over spec solution for customer.
So do you have any other better solution ? Or do you think TPS63806 can support up to 3A ?
Thanks!
Kai