Hi Zack,
I have finally received the boards back from the manufacture. They are not working properly I only get an output of 1V. The manufacture has done x-ray to confirm that the device is properly soldered to the board.
It does not matter if I use 20V or 3.3V, I always get 1V output.
I have not been able to check the register since I need at least 3V for the communication to work.
Any advice on what to do next?
Regards,
Marlon