Other Parts Discussed in Thread: AM3352
Hi Team,
I'm using TPS65217B PMIC.
TPS65217B VIO connected to VLDO1(1.8V).
PGOOD connected to nPWRONRST of AM3352.
nPWRONRST is power domain 3.3V (VDD6SHV)
Often 3 seconds after turning on the system, VLDO1 voltage changed 1.8V to 2.2V. (7 out of 15 sets are 2.2V, 8sets 1.8V)
I2C is not controlled within the system.
When nPWRONRST is power domain 3.3V, VIO is using only 3.3V?
Based on the "SLVU551I", VIO connected to LDO1 is not problem.
Could you help me to debug this issue?
SLVU551I -Powering the AM335x with the TPS65217x