Other Parts Discussed in Thread: LP8758, LP8758-B0
Does the LP8758-E0 support any two parallel outputs?For example, the output is 8A in one way, 4A in two ways, right?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
The LP8758 has the interleaving capability. This feature allows for paralleling but I need to double check and make sure before confirming. It may take up to next week for answering your question.
Regards
Hello,
Thank you for your patience, I will cover for Mahmoud as he had to go out of office unexpectedly.
8A+4A+4A would be LP8758-Dx, however we do not have a variant with that configuration released currently. LP8758-B0 (single voltage output) is the only other currently released phase configuration.
When will the LP8758-DX be released?
Hello,
Sorry, I should have been more clear. There are no current plans for an LP8758-Dx spin release - however I can have someone from our marketing team reach out to you to determine if there is a sufficient business case for a spin release?