Other Parts Discussed in Thread: LM5170
I have several questions regarding the LM5170-Q1.
1. In buck mode, if the UVLO is set above 2.5V, what would LM5170-Q1 behave if there is a surge current (larger than IPK setting) existing on the load side? Does LM5170 have any transient capability or does it just work strictly as a current mode controller?
2. How accurate is the IPK setting is going to be? From the datasheet, I do notice that there is a big variance on the "IPK internal current source" rating and the rest associated parameters. Is this solely temperature dependent or varying a lot from device to device?