Other Parts Discussed in Thread: TPS650861,
I have built a new board and find that [Regulator] is shutting down.
Or
I have built a new board and find that [Regulator] is measuring lower voltage than expected.
What could be the cause?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TPS650864, TPS650860, and TPS650861 all have power fault monitoring for system protection. If any of the enabled regulators exceeds the power fault threshold during normal operation, the PMIC will trigger an emergency shutdown – disabling all regulators simultaneously in order to try to protect the system. A common issue during debug is to notice a rail shutting down due to emergency shutdown but thinking it is the cause, rather than the effect. This can help to identify what is the cause of the emergency shutdown.
During an emergency shutdown, PMIC shuts down all rails simultaneously. After that, PMIC will reload the OTP memory and check the CTL pins for what to do next. If the CTL pin used for enabling the PMIC is tied high, the PMIC will restart the power up sequence and continue looping. For example:

In this example, at the point where the red circles are, the part senses that any one of its outputs is not at the correct power good threshold and started emergency shutdown. After emergency shutdown has completed, it sees that the system has set CTL1 high and it begins the power up process again.
This behavior often leads to two different diagnosis:
Solution:
First, ensure that any regulators that are enabled by the OTP have external components. The most common cause for this issue is unused regulators – see: https://e2e.ti.com/support/power-management/f/power-management-forum/971278/faq-tps650864-what-to-do-with-unused-voltage-regulators-rails?tisearch=e2e-sitesearch&keymatch=tps650864#
Next, to identify where the fault occurred, read the SHUTDNSRC, PWR_FAULT_STATUS1 and PWR_FAULT_STATUS2 registers to identify where the PMIC is detecting a fault and focus the debug efforts there.
For cases where these cannot be read and the issue is occurring during the power up sequence, the best course of action is to take scope shots of the complete power up sequence to confirm it matches the expected sequence from the datasheet or app notes. If a regulator fails to turn on – this can either be the regulator to focus on or the regulator before this may be having an issue.
For cases where these cannot be read and the issue is occurring during normal operation after power up, the best approach is to check the voltage on each regulator with an oscilloscope during the fault – use an oscilloscope to trigger on one of the GPOs (they are set low with a good edge), check the voltage of each regulator right before the GPO goes low – the abnormal rail often shows a rising or falling behavior before triggering the fault.
Regulators to check in order of importance: