Other Parts Discussed in Thread: BQ78350, BQSTUDIO
Hi,
I am trying to communicate with BQ78350-R1 using STM32F091,via SM BUS protocol.
I am getting a NACK after the slave address(0x16), What can be the reason for the NACK?
I am running the clock at 60khz,and clock stretching is enabled. The Cumulative clock low extended time is 4ms. How to know that BQ78530 is ready for communication? The data line and clock line are pulled up to 3.3V using external pull up resistor. The VEN pin is generating pulses of(1.5V) does this indicate that the device is still booting or does it do it even after boot-up? Currently I have powered up BQ78350 using external power source (2.5V).