Other Parts Discussed in Thread: EV2400, ,
Hi,
I am using the BQ25792 as a boost charger for my 3S1P battery charging system. I changed the charging current REG03 register to 3000mA using EV2400 & Battery management Studio. But the charging current is not going more than 1.2A. For example If I set the charging current to 500mA means, it working perfectly, the charging current comes to 500mA. But in my case charging current must be 3A. Help me to solve the problem:
Input: 12V/5A Max
Battery: Li-Ion - 3Series & 1 Parallel
Charging Voltage: 12.6V
Required Charging Current: 3A
Current Situation:
Input Current Max: 1.240A
Battery Charging Current: 1.186A
I attached the register file and schematic.
* Created: Sun Apr 11 19:00:12 IST 2021 * * Format: Register Name tab Character,\t Register Address tab Character,\t Hexadecimal register value. * Device: BQ25790_92 * BQZ Container: Charger_2_00-bq25790_92.bqz * REG00 1A REG01 04EC REG03 012C REG05 6A REG06 0091 REG08 F2 REG09 05 REG0A A3 REG0B 00DC REG0D 4B REG0E 3D REG0F A2 REG10 80 REG11 40 REG12 00 REG13 21 REG14 16 REG15 AA REG16 C0 REG17 7A REG18 54 REG19 0091 REG1B 0F REG1C 6A REG1D 01 REG1E 40 REG1F 00 REG20 00 REG21 00 REG22 00 REG23 00 REG24 00 REG25 00 REG26 00 REG27 00 REG28 00 REG29 00 REG2A 00 REG2B 00 REG2C 00 REG2D 00 REG2E 30 REG2F 00 REG30 00 REG31 0000 REG33 0000 REG35 2F1C REG37 0000 REG37 0000 REG3B 0000 REG3D 0000 REG3F 0000 REG41 0000 REG43 0000 REG45 0000 REG47 00 REG48 08
Regards,
Nishanth M