Part Number: BQ40Z50-R4-DEVICE-FW
I'm going through the Data Memory options, I've updated the 'Calibration' and 'Settings' section to what I want, but when I change the data on the 'Advanced Charge Algorithm' section or those that follow, it wont accept the values. When I try changing the T2 Temp from 12.0 to 5.0 enter the data in a field and try to write the data, I get the error message:
A read of data written failed comparison.
If I then do a 'write all' operation I get the error
Parameter not written. Classname Lifetimes, Subclass name Time, Parameter name Time Spent in UT RSOC H written to data memory faild readback verification.
I've not changed the lifetime data section though
It seems to be similar for all the other fields in the other sections - even manufacturer data.I cannot change the values.
Any ideas? I'm using BQStudio 1.3.86. I've also tried 1.3.104
The device, as far as I know, is unsealed. I flashed in the R4 firmware from the website and all I've changed so far is the Calibration and Settings sections.
Thanks