Hi everyone,
I'm trying to configure the step down TPS54561 in its inverting output voltage mode(Create an Inverting Power Supply from a Step-Down Regulator (Rev. B)) and i'm simulating it in OrCad Capture trough the model available in TI website. Now when simulating the Soft Start node doesn't rise more than 100 mv and after 100 us drops to zero. I'm setting the soft start time to 1 ms. As you can imagine the output voltage doesn't rise to its final value(-18V), starting from a Vin = 24V. So the question is about if the Pspice model is able to simulate the inverting configuration. In the positive voltage mode instead the model works very well.
Thanks in advance,
Samuele.