This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS55288 is damaged when output 20V

Part Number: TPS55288
Other Parts Discussed in Thread: TPS65988DK

hi,

My customer use TPS65988DK + TPS55288 for TBT4 monitor.

when connect type C cable with NB, 988 sends comment to 55288 for 20V output. very soon, 55288 is damaged and Vout is short to ground.

 

I jump wire from customer's main board to TPS55288 EVM. The evm works well. It means that the fw of 988dk is correct and the issue is from their board or layout.

Do you know where I can check?

BR,

frank