Hi team,
If internal soft start of TPS51116 does not meet the requirements in the datasheet, will the corresponding protection mechanisms, such as overvoltage protection, overcurrent protection, etc., be triggered?
Best regards,
Wendy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
If internal soft start of TPS51116 does not meet the requirements in the datasheet, will the corresponding protection mechanisms, such as overvoltage protection, overcurrent protection, etc., be triggered?
Best regards,
Wendy
Hi Wendy,
Can you elaborate what do you mean by internal soft start does not meet requirement in the datasheet?
Regards,
Weidong
Hi Weidong,
For TPS5116, the internal soft-start sequence does not meet the requirement given in datasheet means that connect Pins ‘S3’ and ‘S5’ with Pin ‘V5IN’ together. What’s more, if connect Pin ‘PGOOD’ to external power (3.3V) directly (no any resistors), this wrong connection will trigger internal protection of TPS5116, thus, TPS5116 will not work. Is this description correct?
Hi Wendy,
If you connect S3 and S5 to V5IN, the part should still work. It will power up both VDDQ and VTT when V5IN reach UVLO threshold, and will only turn off when you turn V5IN off.
However, if you connect PGOOD to external 3.3V directly, there is risk of damage the PGOOD pin when PGOOD is logic low. So a pull up resistor is definitely needed.
Regards,
Weidong