This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] TPS53513: PGOOD and MODE pin voltage requirements for TPS53513, TPS53515, TPS53915, and TPS548A20

Part Number: TPS53513
Other Parts Discussed in Thread: TPS53515, , TPS548A20, TPS53915

The TPS53515 is in FCCM when the mode pin is connected to either PGOOD or VREG. What is the minimum voltage requirement for connecting the mode pin to PGOOD?

 The MODE pin needs to be pulled up to at least 2.5V nominal for the device to operate in FCCM.

When pulling up the MODE pin to PGOOD, does the resistor need to be exactly the value listed on the datasheet?

The resistors do not need to be an exact match for the MODE pin pullup. For example, a 10k resistor can be used in place of the 20k recommended, so long as the PGOOD pullup voltage is greater than 2.5V.

How can the voltage to the PGOOD pin be supplied?

The PGOOD pin is open-drain, and should be pulled up to a voltage supply. This can by connecting a resistor (eg. 100k) between PGOOD and either VREG or an external voltage. If an external voltage is used, exercise caution when using a voltage less than 3.3V.  If the external voltage is less than 3.3V, the voltage seen by the MODE pin may be below the 2.5V threshold, depending on the resistors chosen between the reference voltage, PGOOD, and MODE.

What other parts does this guidance apply to?

This guidance also applies to the TPS53513, TPS53515, TPS53915, and TPS548A20 parts.