Hi team,
I got a question from customer.
How do I have to connect the RT-Pin, if I have an external clock on the SYNC/MODE INPUT?
===========================================================================
RT Pin connection in datasheet –JULY 2020: VCC 400 kHz (I dont want 400kHz) AGND 2100 kHz (I dont want 2100kHz) RT to AGND Adjustable according to RT value ( I dont want frequency=f(Resistor)) Float (not recommended) No switching (I dont want no switching)
===========================================================================
I want frequency = External Clock on SYNC/MODE INPUT, because I will have 6x LM63610 on 1 board with phase-shifted Switching on the same frequency of the external clock.
Thanks a lot.
Best regards,