in my application, there is a long conductor between 7rd and 8rd cell,the conductor voltage about 0~800mV,can I use BQ76PL455A-Q1 (VSENSE8 & VSENSE7)to test the conductor voltage?if cannot,do you have good idea?thanks。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
in my application, there is a long conductor between 7rd and 8rd cell,the conductor voltage about 0~800mV,can I use BQ76PL455A-Q1 (VSENSE8 & VSENSE7)to test the conductor voltage?if cannot,do you have good idea?thanks。
Hi David,
Do we have the spec for the maximum time for Vsense channel to survive under -0.3V?
What is the power grade of internal TVS protection in Vsense pin ? Thanks.
Hi Cheng,
Those diodes are for ESD protection and not meant to protect the pin from negative voltages. Customers will sometimes bring this up as a solution, but I do not recommend this at all.