Hello,
Could you please letm e know the difference between bq24296M and bq24296?
I couldn't understand the difference from the datasheet.
Best Regards,
Ryuji Asaka
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Features |
bq24295 |
bq24296 |
bq24297 |
bq24296M |
bq24298 |
Vbus Operation |
3.9-6.2V |
3.9-6.2V |
3.9-6.2V |
3.9-6.2V |
3.9-6.2V |
Maximum Charge Current |
3A |
3A |
3A |
3A |
3A |
Boost Mode Output Current |
1.5A |
1.5A |
1.5A |
1.5A |
1.5A |
USB Detection |
D+/D- |
PSEL |
D+/D- |
PSEL |
PSEL |
BATFET Overcurrent Latch off |
Yes |
Yes |
Yes |
No |
No |
VINDPM Default |
4.76V |
4.36V |
4.36V |
4.36V |
4.36V |
Max. VSYS Regulation Voltage |
VBAT + 150mV |
VBAT + 150mV |
VBAT + 150mV |
VBAT+ 70mV |
VBAT+ 70mV |
Adapter Input Current Limit |
3A |
3A |
3A |
3A |
3A |
Default Precharging Current |
256mA |
256mA |
256mA |
128mA |
128mA |
Default Charging Current |
1.012A |
2.048A |
2.048A |
2.048A |
2.048A |
Termination Current Range |
128mA ~ 2048mA |
128mA ~ 2048mA |
128mA ~ 2048mA |
128mA ~ 1024mA |
128mA ~ 1024mA |
QON |
Low to High Exit Ship Mode |
Low to High Exit Ship Mode |
Low to High Exit Ship Mode |
Low to High Exit Ship Mode |
Hi to Low Exit Ship Mode System reset |
Force BATFET Off Control (I2C) |
Instant-off |
Instant-off |
Instant-off |
Instant-off |
9s delay |
Package |
RGE-24 |
RGE-24 |
RGE-24 |
RGE-24 |
RTW-24 |
Thanks!