Other Parts Discussed in Thread: BQ25895EVM-664
We have the EVM working well, running from a 5V power supply and charging a 10AH cell. The product is primarily mains powered with the battery for backup. The load is connected to the PMID and GND terminals and typical power consumption is around 1 Amp.
Our problem is the 30mS delay in the boost converter starting when the mains power is removed. The voltage on the PMID output is 5V when on mains power and 5.1V when on battery power, but unfortunately dips to about 3V6 on the mains to battery changeover for around 30mS. This is sometimes enough (particularly if the battery is not fully charged) to cause a reset on the attached load.
Is there any way around this?
Thankyou... Chris Jordan