Part Number: BQ24040
Other Parts Discussed in Thread: BQ24090, BQ24072
I have been using both BQ24040 and BQ24090 parts for charging Li-ion pack < 2500mA without issue at 750mA. I have new pack at 3200mA-H and now BQ's are going into thermal shutdown. I have determined it is due to the new packs have a lower initial voltage and now the BQ linear regulator is overheating from the extra input to output voltage drop. Obviously I can reduce fast current limit to reduce power but this will also reduce charge time on these higher capacity batteries. My question to TI support, if these BQ parts go into thermal shutdown until the batteries attain a 3.8V level, will this degrade or harm the chip?