Part Number: BQ24072T
Other Parts Discussed in Thread: BQ24072, , BQ24040
Hello,
Looking at the bq24072T or bq24072, it mentions that the Vout is regulated at Vbat+225mV. The problem is I have a microchip which can only be safely be used between 2.8V to 4.3V.
The thing is I have two types of batteries (3300mAH 3.6V with float voltage of 4.2V and 2600mAH 3.7V with float voltage of 4.2V).
My question is if my battery is charging and reaches full charge that would be 4.2V but the Vout (reg) would regulate is at 4.2V + 225mV (4.425V).
Am I correct in saying that Vout would reach 4.425V when the battery is at full capacity? Or would the peak Vout be less?
I hope to hear from you guys soon.
Best regards
Mohammed Al-Amin