Hello,
I am trying to make use of the BQ24090 as part of a battery pack. I have the chip set up as shown in the attached diagram. J3 is connected to the battery and U11 is not currently connected. When I apply a 5v supply to this circuit with a battery attached no current is drawn and there is no increase in battery voltage. I wonder if anyone has any suggestions. My principal question is if the schematic looks ok as I can't think of any other reason for it not working. For clarity, the battery has a 10K NTC which is connected to the chip.
Any suggestions would be great. Thanks!